DUG_Micro Module Shades Control_WSE-02

Testing the device

Before using the Puck, manually test the Puck and make sure that it works when connected to the shutter.
WARNING
HAZARD OF ELECTRIC SHOCK
  • Observe the regulations for working on live parts.
  • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  • Short press the test button once, the shutter opens/closes gradually.

  • Press and hold the test button, the shutter opens/closes fully, record the time it takes to fully open/close the shutter.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?