DUG_Micro Module Shades Control_WSE-02

Pairing device manually

To pair the device manually:
  1. On Home page, tap + .
  2. Tap and select the Wiser Hub
  3. Select an option to add the device (A):
    • Add Device with Install Code
    • Add Device without Install Code

    TIP: It is highly recommended to add the device with install code.
  4. To pair the device with an install code, tap Add Device with Install Code to display the slide-up menu. Select any one of the options (B):
    • Scan Install Code - you can scan the device for the install code.
    • Enter Install Code Manually - you can manually enter the install code from the device.
    After pairing the device with install code, proceed to Step 6.

  5. To pair the device without install code, tap Add Device without Install Code.
  6. Remove front panel from switch to access the device if you place the puck behind a mechanical push button.
  7. Select any one of the options to add the device:
    • Short press the setup/reset button 3 times (< 0,5 s) on the Puck with a screwdriver.
    • Short press the push button 3 times.

    The LED blinks orange.
    NOTE: If the puck is located behind the push button, the status LED is not visible.
  8. In the app, select Confirm LED is flashing orange and tap Start Configuration (C).

    The app displays the progress of connecting the device.
  9. Wait for a few seconds until the LED turns green. You can also see in the app that the device is joined.

  10. After the device is added in the app, tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?