DUG_Micro Module Shades Control_WSE-02

Troubleshooting

Symptom

Solution

No shutter movement or uncontrolled shutter movement.

  • Check power supply.

  • Check the wiring between Puck and push-button switch..

  • Check the load

The device is not ready to pair after the device is removed from the app.

Reset to factory default settings, refer to Resetting the device

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?