DUG_Micro Module Shades Control_WSE-02

Opening/Closing through device menu

The shutter can be open/close to the desire percentage.
To open/close the shutter:
  1. On the Home page, Tap All devices > Micromodule Shutter.
  2. On the device menu, drag the sliding bar (A) up/down to set the desired shutter opening/closing percentage.
  3. Tap on Open/Mid-Open/Close (B) position to tilt the Slat (Only if the shutter is installed with rotation slat).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?