DUG_Micro Module Shades Control_WSE-02

About the device

The Wiser Micro Module Shades Control (hereinafter referred to as Puck) combines the advantages of smart shutter functionality with ordinary mechanical double push-button switches. It transforms a conventional switch into a connected device that you can control from the switch or through the Wiser app.
Relay contacts are mechanically locked against each other to prevent simultaneous triggering of the two relay outputs.
NOTE: Do not control any devices that depend on a permanent power supply.

Control options

Home control using Wiser Home app: To control the puck through the Wiser app you will need the Wiser Hub. Refer to Pairing the device.

Direct operation: The puck can always be controlled directly on-site. You can also connect it with mechanical double push-button switch. Refer to Manual operation.

Additional features:

  • Remote control with maximum of 10 mechanical double push-button switches.

  • Protection of the motor against damage with two mutually mechanically and electronically locked relay contacts.

  • Electronic overload protection, overheating protection and short-circuit protection.

  • Setting a time schedule.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?