DUG_Wiser Smart Plug_WSE_01

Editing an automation

To edit an automation:
  1. On the Automation tab, locate the automation you want to edit and tap .
  2. On the Edit page, you can tap each item (such as dimmer, shutter, delay, temperature, etc.) to change the settings.
    TIP:
    • You can add one or more actions using .

    • To delete an existing condition or action, slide each item towards left and tap Delete.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?