DUG_Wiser Smart Plug_WSE_01

Checking the power consumption

Using the Wiser app, you can monitor the power consumption of the load connected to the device by accessing the consumption feature.
TIP: You can see the daily real-time power consumption value of the load connected to the device on the control panel of the device.
To see the history of device power:
  1. On the Home page, tap All devices > Smart Plug.
  2. On the device control panel page, tap Consumption.
  3. In the Consumption page, you can see the total power consumption and it’s changes in Week (A), Month (B), and Year (C) view in the graph.
    You can tap each bar on the graph to see the total power consumed on a particular day/month.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?