DUG_Wiser Smart Plug_WSE_01

Example of an automation

This demonstration shows you how to create an automation to get notification on your app when the total power consumption of the device connected to the Plug is 50 kWh.
  1. Go to Automation > + to create an automation.
  2. Tap Edit name, enter the name of the automation and tap Save.
    TIP: You can choose the cover image that best represents your automation by tapping .
  3. Tap Add Condition > When device status changes > Smart Plug.
  4. Tap Daily Consumption, select the total power consumption value (A) and tap Next.
    TIP: You can set the power consumption value as 50 kWh.

  5. Tap Add task > Send notification and select Notifications (B) then tap Next.

  6. In the Automation Settings page, tap Save.

    Once the automation is saved, it is visible on the Automation tab. You can tap the toggle switch on the automation to enable it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?