DUG_Wiser Smart Plug_WSE_01

Pairing the device

Using the Wiser app, first pair your device with the Gateway to access and control the device. You can either add the device manually or do an auto-scan to pair it.
NOTE: The Plug shows a non-zero power consumption value when the device is added to the app if the Plug was in ON state with a load connected before pairing it to the Gateway.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?