DUG_Wiser Smart Plug_WSE_01

About the device

The Wiser Smart Plug (hereinafter referred to as Plug) is used as a plug adapter to control various electrical devices such as floor lamps, radios, ventilators or coffee machines manually or using Wiser app. The plug can also monitor energy consumption of plugged-in devices. The wall socket needs to be switched On for it to function.
NOTE: Do not insert the plug into socket outlets that are behind large objects or furniture such as refrigerators or cabinets that reduces the radio reception.

Control options

Home control: To control the plug in your home through the Wiser app you will need the Wiser Gateway.

Direct operation: The plug can always be controlled directly on-site. To do this, you can switch the plug On and Off with the operation button.

Functions

  • Switching On and Off plugged-in devices manually and remotely via app.

  • Setting a timer or a time schedule (via app)

  • Visibility of load status (via app)

  • Monitoring and visualization of energy consumption (via app)

Operating elements

  1. A: Socket for protective earthing and standardized European plugs

  2. B: Status LED

  3. C: Operation button

  4. D: Plug fitting to a European protective earthing socket outlet

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?