DUG_Exxact Connected Motion Sensor with Switch 10 A_WH-00

Switching On/Off the device manually

You can turn on/off the Motion Sensor Switch manually.

Short press the push button (< 0,5 s) once to turn on/off the Motion Sensor Switch.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?