DUG_Exxact Connected Motion Sensor with Switch 10 A_WH-00

Turning On/Off device using app

  1. On the Control tab, tap All devices or the room tab where the device is located.
  2. Tap (A) to turn on/off the device.
    NOTE: The Control tab will not be visible if you have only a single device in the Wiser System. All functions will be accessible through the Home screen.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?