Configuring the device
|
A |
Device Name: Tap to change the name of the device. |
|
B |
Location: Tap to assign the device to any room (such as living room, bedroom, kitchen etc). For more information, refer to Setting the device location. |
|
C |
Motion Detection Sensitivity: Tap to set the sensitivity level of the sensor as per your preference. For more information, refer to Setting the detection sensitivity for detailed information on each option. |
|
D |
Motion Detection Timer: Tap to set the time for how long the light should remain On after motion is detected. For more information, refer to Setting the motion detection timer. |
|
E |
Current Lux: Displays the current Lux value of the light present in the environment measured by the sensor. Lux is a unit of illuminance that measures the amount of visible light present in an area. It helps the sensor determine how bright or dark the environment is. |
|
F |
Lux Level Threshold: Tap to set the threshold value for Lux ranges that determine when the sensor should activate. For more information, refer to Defining Lux settings. |
|
G |
Notify me if motion is detected: Tap the toggle switch to receive notifications when motion is detected. |
|
H |
Identify: Tap
to identify the device. The status LED blinks red and the connected
light blinks on and off, upon successful identification. |
|
I |
Delete: Tap to remove the device from the system. NOTE:
|
|
J |
Zigbee Signal Strength Indicator: Zigbee Signal Strength indicator which displays the current signal strength of the device. |