DUG_Exxact Connected Motion Sensor with Switch 10 A_WH-00

Troubleshooting

Symptom

Solution

Load does not switch on automatically.

Increase the detection sensitivity in device settings.

Check the Lux value. If the ambient Lux level is higher than the threshold, the light will not turn on.

Load does not switch off automatically when an automation is triggered.

Reduce the action delay time.

Connected load does not switch on.

  • Check the power supply.

  • Turn the device off and back on again.

  • Check the load.

  • In the case of an external push button, check the wiring.

The device is not ready to pair after the device is removed from the app.

Reset to factory default settings, refer to Resetting the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?