DUG_Exxact Connected Motion Sensor with Switch 10 A_WH-00

About the device

The Connected Motion Sensor with Switch 10 A (hereinafter referred to as Motion Sensor Switch) detects moving heat sources (e.g. persons) and can switch on ohmic, inductive or capacitive loads for a settable overtravel time.

Control options

Home control: To control the motion sensor switch through the Wiser Home app you will need the Wiser Hub.

Direct operation: The motion sensor switch can always be controlled directly on-site. You can also connect any number of mechanical push-buttons.

Functions

  • Detection range.

  • Automatic mode, manual operation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?