DUG_Exxact Connected Motion Sensor with Switch 10 A_WH-00

Google Home

You can use Google Assistant to request information or perform an action using a variety of commands.

Common Wiser commands for Google Home:

  • Inquiry: “OK, Google, is the Motion Sensor Switch On?”

  • Motion detection: “OK, Google, is the sensor detecting movements?”

  • Turn on/off the device: “OK, Google, turn on/off the Motion Sensor Switch.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?