Assigning an Action to the Wireless switch
To configure an Action to the Wireless switch:
-
On the Control tab, tap All devices or the room tab where the Wireless switch is located.
-
Tap any key and select Action.
-
Select the device and tap Select Action.
-
On the Configure Device screen, select the Light Switch.
- Tap
to turn on the light and tap .
In the next screen,
shows that the Action is successfully configured.
The Top Left key is configured with Light Switch: On.
TIP: When assigning a push button to control a dimmer or a shutter, it is important to know that you can set a specific percentage for brightness or shutter position. For example, if you configure a dimmer to 50%, short pressing the push button will turn on the light directly at 50% brightness. Similarly, for shutters, you can set a position to 30% open. When you short press the push button, the shutter will automatically move to that position.NOTE: Pressing and holding the push button cannot dim the light or open/close the shutter.