DUG_LK FUGA Wiser Wireless Switch_WH-00

About the device

The LK FUGA® Wiser wireless battery 4 button switch (hereinafter referred to as Wireless switch) is a battery-powered wireless switch that is used to control a group of Zigbee devices (such as light and shutter) within the same Zigbee network.

The Wireless switch can be configured through the Wiser Home app.

IMPORTANT: The push-button pair is arranged horizontally on the Wireless switch.

Advantage of using a Wireless switch:

  • Easy to use and user-friendly interface: also good for children (placed lower on the wall) and for the elderly who may not be so familiar with smart phones.

  • Easy to mount on the wall: no wiring required.

Features of a Wireless Switch:

  • Add various actions (such as lighting/shutter control) to the Wireless switch.

  • Control a group (such as lighting and shutter control).

  • Add moments to the Wireless switch (such as Movie Night Moment/Good Night Moment).

  • Low battery notification.

NOTE: The signal strength can be affected by environmental factors and construction materials, which may cause interference between the Wiser Hub and connected devices.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.