DUG_LK FUGA Wiser Wireless Switch_WH-00

Controlling the device with Push Buttons

After assigning an Action/Moment to the Wireless switch, you can operate it by pressing the push buttons.

Light

Short press the assigned push button on the Wireless switch (< 0,5 s) to turn the light on/off, or set it to a specific brightness level ( for dimmers only).

Shutter

Short press the assigned push button on the Wireless switch (< 0,5 s) to open/ close the shutter to the configured percentage.

Moment

Short press the push button to activate a Moment.

TIP: You can configure the Wireless switch push buttons with Action/Moment/Group using the app.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?