DUG_Mureva EVlink_Socket_WH-05

Creating a schedule

Schedules can control the charging process of Mureva EVlink Socket. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time.
  1. On the Control tab, tap All > Mureva EVlink Socket.
  2. Tap Charging Mode.
    NOTE: If you have Mureva EVlink Socket installed with Wiser Hub you can also navigate the following path to create schedules:
    • On the Home screen, tap .

    • Tap Schedules > EV schedule. Proceed with step 3.

  3. On the EV Charging Mode page, select Customized Schedule.
    NOTE: The Mureva EVlink Socket will have a default schedule pre set to the user. You can edit the schedule as required.
    IMPORTANT: It is required to set an On and Off state for a schedule.
  4. Select days (A).
  5. Tap (B) to edit the schedule.
  6. Select a state (On/Off) (C), time period (D) and tap Set.
    TIP:
    • You can add multiple schedules based on your requirement. Select days (A), tap (E), set On/Off state and time.

    • You can copy the existing schedule to the days of your choice. Tap (F), select the days and tap Copy.

    • When the schedule begins, you can see the until time in the following screens:

      • Device Control Screen.

      • Control tab under the device name.

      • Favourite devices section on the home screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?