DUG_Mureva EVlink_Socket_WH-05

Changing device lock

Using the Wiser Home app, you can enable or disable the local control via push-button.
  1. On the Control tab, tap All > Mureva EVlink Socket > Device settings.
  2. Enable or disable the Device Lock (A) as required.
    The settings will be saved automatically. When the device is locked, (B) is displayed next to the device image.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?