DUG_PTC_WH-03

Example of an automation

This demonstration shows you how to create an automation to controlling a hot water system when solar production is greater than 2 kW.
NOTE: If your home location is in Belgium, Denmark, Sweden, and Finland. Make sure to install PowerTag Energy and pair it with the Wiser Home system to create and perform an automation.
TIP: It is mandatory to create two automations. First, turn on the hot water system when the solar production is greater than 2 kW. Second, turn off the hot water system when the solar production is less.
The hot water system will not turn off automatically until you create another automation.
  1. Go to Automation > to create an automation.
  2. To add a condition, tap Add Condition > Device status change > Solar Panel.
  3. Set the production power to 2 kW (A) and the condition as more than (B) and then tap Set.
  4. Read the information and tap OK.
  5. To add an action, tap Then > Add an action > Control a device > Heating. Set device state as On and then tap Set located on the upper right corner.
    NOTE: By default, the state is set to Off.
  6. Enter the name of the automation.
    TIP: You can choose the cover image that represents your automation by tapping .
  7. Tap Save.Once the automation is saved, it is visible on the Automation tab.
    NOTE: You can enable or disable saved automations on the Automations tab by using .
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?