DUG_PowerTag-E_WH-10

Creating/updating home profile

User must create a home profile to compare the energy consumption with similar home profiles and also to get the energy usage breakdown based on categories like heating, cooking, lighting, washing etc.
To create home profile:
  1. On the Home Profile page tap Continue.
  2. Select the type of home you live and tap Next.
    NOTE: Based on the type of home step 4 to step 12 may differ.
  3. Set the size of your home either by tapping (A) or using the sliding bar (B).
    NOTE: Maximum home size can be 400 sq m.
  4. Set the number of people living in the home either by tapping (C) or using the sliding bar (D).
    NOTE: Maximum 10 people can be added.
  5. Select the main heating system and tap Next:
    • Radiators
    • Air/Air Heat Pump
    • Air/Water Heat Pump
    • Ground Source Heat Pump
    • District Heating
    • Pellet Stove
    • Gas
    • Other
  6. Select the type of hot water system and tap Next:
    • District Heating
    • Water Heater (Water Pan)
    • Air Water Heat Pump
    • Ground Source Heat Pump
    • Gas
    • Other
  7. Select the appliances used to cook and tap Next:
    NOTE:
    • By default it will be 0, use +/- to set the number.

    • Maximum of 5 individual appliances can be added.

  8. Select the appliances in your home and tap Next:
    • Dishwashers
    • Washing Machines
    • Dryers
    • TVs
    • Game Consoles
    • Laptops
    • Stationary Computers
    NOTE: Maximum 5 individual appliances can be added.
  9. Select the fridges and freezers from the list:
    • Fridges
    • Freezers
    • Fridges and Freezers
    NOTE: Maximum 5 individual appliances can be added.
  10. Select the number of Electric cars and tap Next.
  11. Select the air conditioners from the list and tap Done.
    • Air/Air Heat Pump
    • Air/Water Reversible Heat Pump
    • Other
    NOTE: To update the home profile, on the Insights tab, tap Update my home profile, follow from step 2.
    To view history and insights of estimated energy consumption of similar homes, refer to Personalized Energy Insights (Estimated energy).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?