DUG_PowerTag-E_WH-10

Enabling Personalized Energy Insights

Using the Wiser Home app you can enable Personalized Energy Insights to monitor the energy breakdown, and comparison between similar homes and also view energy-saving tips.
IMPORTANT: To enable Personalized Energy Insights you must configure one PowerTag as Grid (main incomer).
NOTE:
  • You will be notified that this feature is available after PowerTag is commissioned.

  • You can enable this feature and create your home profile.

  • You should have minimum of 1 month of load consumption data to view your energy breakdown. A push-notification will be sent to the user when data is available.

To enable Personalized Energy Insights:

  1. On the Home screen, tap Energy Dashboard > Insights, then tap splash screen (A).
    NOTE: Do not accidentally close the splash screen as it will take 2 weeks and a final reminder after 6 weeks to reappear.
  2. Read the tutorial information and tap Next twice, then tap Unlock Energy Insights.
  3. Read the privacy notice and tap Activate on each page.
    NOTE: Accepting consent is optional.
  4. Once Personalized Energy Insights is successfully enabled, you will receive an in-app notification and then immediately you will be prompted to create a home profile. Refer Creating home profile.
    NOTE: You can also navigate through in-app notification which is received after enabling Personalized Energy Insights by tapping .
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?