Showing 151 - 160 of 1,622 results

Page 16 of 163
  • Om enheden

    Wiser rumtermostat – Brugervejledning til Wiser Home-enheden

    , batteriniveau, boost-status, varmesymbol og signalstatus. På rumtermostatens skærm ændres ikonet og vises , når rummet er i komfort-tilstand, og når rummet er i øko-tilstand. Du kan finde flere oplysninger i systembrugervejledningen. Fordelen ved at bruge rumtermostaten: Let at styre alle
  • Updating the Installer Portal

    Schneider Inverter and Boost – Wiser Home Device user guide

    the left menu, click ⊕ Add Site. Enter the required information and then click Add Site. Change the language from the menu in the top right. Configuring export mode By default, zero export mode is enabled. In zero export mode, the Schneider Inverter does not export any power to the grid. The maximum
  • Acerca de Schneider Inverter y Boost

    Schneider Inverter y Boost – Guía del usuario del dispositivo Wiser Home

    Acerca de Schneider Inverter y Boost Acerca de Schneider Inverter y Boost Acerca de Schneider Inverter y Boost Schneider Inverter El Schneider Inverter es un inversor de alto rendimiento monofásico y trifásico con alta eficiencia de conversión que alimenta su hogar y consigue ahorrar en las
  • Creating an automation

    Wiser 16 A Relay for Temperature Control – Wiser Home Device user guide

    Add conditions and select any of the following (C): Device status change: Select a device to enable automation. Away Mode: Enable/Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about Away
  • Aktivitet og omgivelser

    Wiser Home – Systembrugervejledning (Danmark)

    varmen, tælles med et manuelt boost eller boost ned. Antallet af gange, som du har skruet op for varmen, tælles med et boost op eller en manuel justering af temperaturen. Antallet af solskinstimer beregnes som antal timer, hvor skydækket var mindre end 50 %.
  • Schneider Inverter y Boost

    Guía del usuario del dispositivo Wiser Home Schneider Inverter y Boost Información sobre las características y la funcionalidad del dispositivo. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison Francia +33 (0) 1 41 29 70 00 www.se.com DUG_Inverter and Storage_WH-03 10/2025 2024 2025
  • Wiser Flush-mounted Thermostat 2 A

    in Automation such as Boost All, Cancel all overrides and Away mode. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Boost All Boost All You can apply a boost of +2 °C for 1 hour to every room in the system. It won’t affect hot water in any way
  • Activity and environment

    Wiser Home – System User Guide (Denmark)

    you turned your heating down is counted by a manual boost or boost down. Number of times you turned your heating up is counted by a boost up or manual adjustment to the temperature. Number of hours of sunshine is calculated as number of hours when the cloud coverage was less than 50%.
  • Ajuste de la temperatura de la habitación usando la aplicación

    Termostato Empotrado Wiser 2 A – Guía del usuario del dispositivo Wiser Home

    Favoritos. Para obtener más información sobre Favoritos, consulte el tema Gestión de favoritos en la correspondiente guía del usuario del sistema. Al pulsar se puede ajustar el tiempo de Boost y después se apaga cuando termina el tiempo de Boost. Cuando se ajusta el tiempo de Boost, el sistema aumenta
  • Manuelle Einstellung der Raumtemperatur

    Wiser Heizkörperthermostat – Wiser Home Geräte-Benutzerhandbuch

    erhöhen. Die rote LED leuchtet für 5 Sekunden. In „ -“ Richtung, um die Temperatur zu senken. Die blaue LED leuchtet für 5 Sekunden. Durch Drehen der Thermostatkappe erhöhen/verringern Sie die Solltemperatur um 2 °C bezogen auf die aktuelle Raumtemperatur. Der Boost ist 1 Stunde lang aktiv. Liegt die Solltemperatur bereits um mehr als 2 °C über oder unter der Raumtemperatur, ändert sich die Solltemperatur nicht durch einen Boost.
Page 16 of 163