Showing 4,541 - 4,550 of 9,846 results

Page 455 of 985
  • Turning On/Off device using app

    Exxact - Connected Relay Switch 10 A – Wiser Home Device user guide

    Turning On/Off device using app Turning On/Off device using app Turning On/Off device using app On the Control tab, tap All devices or the room tab where the device is located. Tap (A) to turn on/off the relay switch. You can also turn the device on/off from the Home screen when you add it to your Favourite. The Control tab will not be visible if you have only a single device in the Wiser System. All functions will be accessible through the Home screen.
  • About the device

    Exxact - Connected Motion Sensor with Switch 10 A – Wiser Home Device user guide

    About the device About the device About the device The Connected Motion Sensor with Switch 10 A (hereinafter referred to as Motion Sensor Switch) detects moving heat sources (e.g. persons) and can switch on ohmic, inductive or capacitive loads for a settable overtravel time. Control options Home
  • Ställa in enhetsplats

    Exxact – Rörelsedetektor med tryckknapp 10 A uppkopplad – Bruksanvisning för Wiser Home-enhet

    konfigurationsskärmen. På skärmen Inställning av enhet kan du ange Nytt rumsnamn (A) eller välja ett befintligt rum i listan (B). Om enheten redan är tilldelad kan du ta bort den från det befintliga rummet. Tryck på Ta bort från rummet (C). När ändringarna är klara trycker du på Skicka (D).
  • About the device

    Unica - Connected Motion Sensor with Switch 10 A – Wiser Home Device user guide

    About the device About the device About the device The Connected Motion Sensor with Switch 10 A (hereinafter referred to as Motion Sensor Switch) detects moving heat sources (e.g. persons) and can switch on ohmic, inductive or capacitive loads for a settable overtravel time. Control options Home
  • Repor o dispositivo

    Unica - Detetor de movimento variador LED conectável – Guia do utilizador do dispositivo Wiser Home

    Repor o dispositivo Repor o dispositivo Repor o dispositivo Pode repor manualmente o dispositivo para as predefinições de fábrica. Pressione ligeiramente o botão de pressão três vezes (< 0,5 s) e depois pressione demoradamente o botão de pressão uma vez (> 10 s).Ao fim de 10 s, o LED pisca a
  • Datos técnicos

    Unica - Detector de movimiento con regulador LED conectado – Guía del usuario del dispositivo Wiser Home

    reductor 14-150 VA Standby Máx. 0,4 W Conductor neutro No necesario Terminales de conexión Bornes a tornillo durante máx. 2 x 2,5 mm², 0,5 Nm Unidad de extensión Pulsador individual, número ilimitado, máx. 50 m Protección por fusible Interruptor automático de 16 A Frecuencia de funcionamiento de 2405 a 2480 MHz Potencia de radiofrecuencia máx. transmitida <10 mW Protocolo de comunicación Certificación Zigbee 3.0
  • Technical Data

    LK® One Wiser Motion Sensor with Switch 10A – Wiser Home Device user guide

    load 10 A, 140μF Standby Maximum 0.4 W Connecting Terminals Screw terminals for max. 2 x 2.5 mm², 0.5 Nm Extension unit Single Push-button, unlimited number, max. 50 m External fuse protection 16 A circuit breaker Nominal current 10 A, cosφ = 0.6 Operating frequency 2405 - 2480 MHz Max. radio-frequency power transmitted < 10 mW Communication protocol Zigbee 3.0 certified
  • Indicaciones LED

    Enchufe inalámbrico Wiser 16A – Guía del usuario del dispositivo Wiser Home

    se ilumina en verde durante un tiempo antes de apagarse. Restablecimiento Acción del usuario Indicación mediante LED Estado Pulse el botón de funcionamiento 3 veces y manténgalo pulsado una vez durante > 10 s. Después de 10 s, el LED empieza a parpadear en rojo. El dispositivo se encuentra en
  • Operaciones de conmutación mediante la aplicación

    Enchufe inalámbrico Wiser 16A – Guía del usuario del dispositivo Wiser Home

    Operaciones de conmutación mediante la aplicación Operaciones de conmutación mediante la aplicación Operaciones de conmutación mediante la aplicación Puede encender/apagar el enchufe de forma remota usando la aplicación Wiser Home. Vaya a la pestaña Control, pulse Todos los dispositivos o la
  • About the Document

    Wiser Underfloor Heating Controller / Connection Strip – Wiser Home Device user guide

    corporate strategy for constant improvement, we may revise the content over time to enhance clarity and accuracy. If you see a difference between the characteristics in this document and the characteristics on www.se.com, consider www.se.com to contain the latest information. For your safety HAZARD OF
Page 455 of 985