DUG_EVlink_WH-07

Pairing the device to Wiser Home app

IMPORTANT: Make sure that the EVlink Home Smart has been configured by an electrician.
To pair the device:
  1. On the Home page, tap  .
  2. Tap Devices >  >  Energy.
  3. Select EVlink Home Smart.
    TIP: You can also navigate by tapping Control > > Energy > EVlink Home Smart.
  4. On EVlink Home Smart Setup page, tap Next.
  5. Tap Open camera to scan QR code on your EVlink terminal.
    A notification window will prompt you to authorize Wiser Home to access your camera.
  6. Tap OK.
  7. Point the camera and scan the QR code near the charging socket/connector dock.
    You need to wait for up to 5 minutes for the EVlink Home Smart to join the setup.
  8. If you wish to name the EVlink Home Smart, tap and enter a name.
    NOTE: By default, the name will appear as EVlink Home Smart.
  9. Tap Next and then tap Finish.

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

    Now, you can see the newly added device on the Control tab under the All and Room tabs.

    NOTE: If you only have an EVlink Home Smart in the Wiser System, the Control page will not be visible. All functions will be accessible through the Home page.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.