Showing 4,581 - 4,590 of 9,846 results

Page 459 of 985
  • LED indications

    Odace - Connected Wireless Switch 1-gang/ 2-gang – Wiser Home Device user guide

    LED indications LED indications LED indications Pairing the device User Action LED Indication Status Press the push button 3 times. LED blinks orange, once per second. Pairing mode is active for 30 seconds. When pairing is completed, LED displays solid green for a few seconds, before turning Off
  • Caractéristiques techniques

    Ovalis - Prise de courant connectée 16A – Guide de l'utilisateur de l’appareil Wiser Home

    Caractéristiques techniques Caractéristiques techniques Caractéristiques techniques Puissance nominale du type de charge Lampe incandescente 2000 W LED 100 W, 12 µF Transformateur à noyau de fer 1500 VA Moteur 1 600 VA, max 7 A Convertisseur abaisseur de tension électronique 2000 VA Résistance 3680
  • Turning On/Off device using app

    Unica - Connected Relay Switch 10 A – Wiser Home Device user guide

    Turning On/Off device using app Turning On/Off device using app Turning On/Off device using app On the Control tab, tap All devices or the room tab where the device is located. Tap (A) to turn on/off the relay switch. You can also turn the device on/off from the Home screen when you add it to your Favourite. The Control tab will not be visible if you have only a single device in the Wiser System. All functions will be accessible through the Home screen.
  • Informações técnicas

    Sistema M e Sistema D - Tomada conectável 16A – Guia do utilizador do dispositivo Wiser Home

    Informações técnicas Informações técnicas Informações técnicas Potência nominal para o tipo de carga 2000 W 100 W, 125 µF 1500 VA 2000 VA 3680 W 6 AX, máx. 70 µF 16 A, cos φ = 0,6 1600 VA, máx 7 A Tensão nominal: CA 230 V~, 50 Hz Stand-by: máx. 0,4 W Proteção de fusíveis: Disjuntor 16 A Terminais
  • Operaciones de conmutación mediante la aplicación

    System M y Sistema D - Toma de corriente inteligente, 1 elemento, 16 A – Guía del usuario del dispositivo Wiser Home

    Operaciones de conmutación mediante la aplicación Operaciones de conmutación mediante la aplicación Operaciones de conmutación mediante la aplicación Con la aplicación Wiser Home, puede encender/apagar la toma de corriente de forma remota. Encender/apagar la toma de corriente: Vaya a la página
  • Utilizar o dispositivo

    PowerTag Control – Guia do utilizador do dispositivo

    Utilizar o dispositivo Utilizar o dispositivo Utilizar o dispositivo O Painel de Controlo permite-lhe ligar e desligar o dispositivo e controlar várias definições. No separador Controlo, toque em Todos os dispositivos ou num separador de divisão onde está a tomada, um ícone para abrir o ecrã
  • Setting-up Overconsumption Alarm

    Wiser Home – System User Guide (Belgium)

    Setting-up Overconsumption Alarm Setting-up Overconsumption Alarm Setting-up Overconsumption Alarm This topic explains how to setup an overconsumption alarm for a device. On the Notifications and Alarms screen, tap Create a new alarm (A). Choose alarm type as Overconsumption (B). Select the device
  • LED indications

    Exxact – Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    LED indications LED indications LED indications Pairing the device User Action LED Indication Status Press the top-right push button 3 times. LED blinks orange, once per second. Pairing mode is active for 30 seconds. When pairing is completed, LED displays solid green for a few seconds, before
  • Using the device

    LK FUGA Wiser Push-button Switch – Wiser Home Device user guide

    Using the device Using the device Using the device The Device Control Screen allows you to switch on/off the device and control various settings. On the Control tab, select the relay switch. The Device Control Screen displays the following options: A Tap to turn the device on/off. B Tap to open the
  • Using the device

    LK One Wiser Push-button Switch – Wiser Home Device user guide

    Using the device Using the device Using the device The Device Control Screen allows you to switch on/off the device and control various settings. On the Control tab, select the relay switch. The Device Control Screen displays the following options: A Tap to turn the device on/off. B Tap to open the
Page 459 of 985