Commissioning via eSetup for Sectorcoupling
For installation, refer to installation instruction.
To download the app, scan below code or click on the link
|
For iOS Search term: Wiser Home https://apps.apple.com/app/wiser-heat/id1222853887 |
For Android Search term: Wiser Home https://play.google.com/store/apps/details?id=com.schneider_electric.WiserHeat |
To commission the inverter:
- Open eSetup app, tap
- Read the safety warning.
- Tap Acknowledge and Continue to continue with the setup.
- Tap Next to confirm energy meter installation and commissioning.
- Make sure all the cables are connected correctly to the inverter according to the Installation Guide and then tap Next.
- Plug the dongle to the inverter and rotate the fastener of the connector to lock the dongle, and then tap Next in the eSetup app.
- Turn on the inverter to activate Bluetooth.
Refer to Installation Guide.IMPORTANT:-
If the dongle's LEDS are not lit after the inverter is turned on, remove and then reconnect the dongle to the inverter.
Once plugged in, the “PWR” and “COM” lights on the dongle will be solid green. -
The Bluetooth connection times out after 30 mins of inactivity. To reactivate, remove and then reconnect the dongle to the inverter.
-
- To connect with the Inverter, select any one of the options:
- Enter the code Manually: manually enter the 12 character alphanumeric serial number located below the barcode.
- Scan Barcode : scan the barcode located on the side of the inverter. Make sure to enable camera permissions in the app settings.
Wait a few seconds for the app to establish a connection with the inverter.
App shows Connected on successful pairing.IMPORTANT: The Bluetooth connection times out after 30 minutes of inactivity. To reactivate, remove and then reconnect the dongle to the inverter.NOTE: Refer to troubleshooting, if you are unable to pair with the inverter. - To create a new PIN, type the new PIN and then re-enter
to confirm. Tap Confirm.TIP:
-
The PIN must contain 6 to 16 digits.
-
Must not have 6 sequential digits in ascending or descending order.
-
Must not the same digit more than 3 times.
NOTE: If a PIN has already been created, you will be prompted to enter the PIN and then tap Confirm.NOTE: If you forgot your PIN, refer to resetting PIN using eSetup app. -
- Once the PIN has been successfully created, the app starts
to detect the connected devices.
Once all devices are detected, tap Next to continue.TIP: If any device is not detected, tap Search again. Make sure the device is turned on. - The app checks if any firmware upgrade is required.
- If there is no firmware upgrade required, skip this step.
- If the devices requires a firmware upgrade follow below steps:
-
Tap Upgrade all devices and connect to your Wi-Fi network.
-
On the dongle, check if the SRV green LED is turned on. If yes, tap It’s Green, If it's not green, check the Wi-Fi connection.
-
Wait for few minutes for the app to download and upgrade all the devices with required firmware update.
When the update is complete, tap OK. The Schneider Inverter will reboot to complete the firmware update. -
Re-enter the PIN and tap Confirm.
-
NOTE: Refer to troubleshooting, if you are unable to connect with the dongle.NOTE: Refer to Compliance with local regulations for details on the minimum firmware version requirements for inverters installed in Germany. - Select export configuration and tap Next.
- Check that power is flowing through the inverter's auxiliary devices. Check the device details, and then tap Next.
- Choose a Wi-Fi Network or tap Enter Wi-Fi Manually. Enter the credentials, and tap Confirm to connect the inverter.
- Wait a few seconds for the app to establish a connection. On the dongle, check if the SRV green LED is turned on, if yes, tap It’s Green. If it's not lit, check the Wi-Fi connection.
- Enter the details of the location where the inverter is commissioned and tap Generate commissioning report.
- Once the report is generated, share the report, or download it for future reference. Tap Done.
- Read and check the checklist and tap Close to complete the commissioning process.
Refer to pairing the device to the complete home owner commissioning process.