Showing 5,301 - 5,310 of 9,846 results

Page 531 of 985
  • Removing the device from the system

    System M and System D - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    Removing the device from the system Removing the device from the system Removing the device from the system Using the Wiser Home app, you can remove the Socket outlet from the Wiser system. To remove the Socket outlet: On the Home page, tap . Tap Devices Connected Socket Delete (A).
  • Technical Data

    Odace - Connected Blind Control Switch – Wiser Home Device user guide

    External fuse protection 10 A circuit breaker Nominal current 4 A, cosφ = 0.6 Operating frequency 2405 - 2480 MHz Max. radio-frequency power transmitted < 10 mW Communication protocol Zigbee 3.0 certified
  • Identifying the device

    Odace - Connected Thermostat 2 A – Wiser Home Device user guide

    Identifying the device Identifying the device Identifying the device Using the Wiser Home app, you can identify the thermostat from the other available devices in the room. On the Home screen, tap . Tap Devices Identify (A). The thermostat LEDs on the dot-matrix display flash white while the wireless connectivity LED flashes green at the same until you tap Ok.
  • Removing the device

    Wiser Power Micromodule – Wiser Home Device User Guide

    Removing the device Removing the device Removing the device Using the Wiser Home app, you can remove the module from the system. To remove the device: On the Home screen, tap . Tap Devices Power Micromodule Delete (A). Tap Remove from System. Removing the device will delete all the historical data
  • Selecting the device location

    Wiser Micromodule for Fil Pilote radiators – Wiser Home Device User Guide

    Selecting the device location Selecting the device location Selecting the device location Using the Wiser Home app, add the device to any room (such as living room, bedroom,etc). On the Home screen, tap . Tap Devices Climate FIP Micromodule Location (A) to assign the device to an existing room or a new room and tap Submit. Tap Remove from Room to remove the device from the existing room.
  • Historia

    Wiser Home – Järjestelmän käyttöopas (Ruotsi, Suomi)

    vuodet), napauta (A). Vihreät palkit osoittavat aurinkoenergian tuotannon ja harmaat palkit näyttävät akun käytön. Napauta ja valitse Kuorman kulutus, kun haluat tarkastella yksittäisten kuormien kuluttamaa energiaa. Napauta (A) uudelleen ajanjakson valitsemiseksi.
  • Redigera en automation

    Wiser Home – Systemanvändarhandbok (Sverige, Finland)

    Redigera en automation Redigera en automation Redigera en automation På skärmen Automation (A): Tryck på automationen som du vill redigera (B). På skärmen Redigera automation kan du: Ändra ikonen. Byt namn på automatiseringen. Ändra villkor, tid eller åtgärd. Så här ändrar du villkor, tid eller
  • Utilizar o dispositivo no Quick Home Connect

    Sensor de Movimento de Exterior ARGUS 360 – Guia do utilizador do dispositivo Wiser Home

    Utilizar o dispositivo no Quick Home Connect Utilizar o dispositivo no Quick Home Connect Utilizar o dispositivo no Quick Home Connect Quando o movimento é detetado na área de deteção do sensor, irá ligar automaticamente a carga conectada (luz). A luz permanecerá ligada durante o período especificado na definição de tempo. Para mais informações, consulte Definições do dispositivo.
  • Om enheten

    Exxact – Uppkopplad rums-/golvtermostat 16 A – Användarhandbok för Wiser Home-enheter

    Om enheten Om enheten Om enheten Den uppkopplade rums-/golvtermostaten 16 A (nedan kallad cFMT/termostat) används främst för elektrisk golvvärme eller elektriska element, men kan även användas för att styra motordrivna ventiler eller cirkulationspumpar för vattenbaserad uppvärmning
  • Laitteen lisäasetukset

    Exxact - Huone/lattiatermostaatti 16 A ZB – Wiser verhokytkin -laitteen käyttöopas

    asettaa kiertoajan ja universaalin tulon. Lisäasetusten muuttaminen voi vaikuttaa vakavasti järjestelmään, joten on tärkeää ymmärtää muutosten vaikutus lisäasetuksiin ennen niiden tekemistä.Lisäasetusten tekeminen: Valitse aloitusnäytössä . Napauta Laitteet Yhdistelmätermostaatti Huoneen asetukset Lisäasetukset (A). Lue huomio ja napauta OK.
Page 531 of 985