Showing 5,761 - 5,770 of 9,846 results

Page 577 of 985
  • Exxact – Multiwire LED-säädin ZB Wiser Home -laitteen käyttöopas

    . Himmentimen käyttäminenVoit kytkeä himmentimen päälle/pois päältä tai säätää sen kirkkautta pariliitoksellayhdistetyn langattoman painikkeen avulla.• Kytke kytketty kuorma (A) päälle/pois päältä painamalla lyhyesti (< 0,5 s) langattoman painikkeen ylä- tai alapainiketta.• Paina pitkään langattoman
  • Einstellen der Geräteplatzierung

    Wiser Funkempfänger 16 A für Temperaturregelung – Benutzerhandbuch des Geräts

    Sie auf Geräte Heizung 16A Relais Position (A), um das Relais dem vorhandenen oder einem neuen Raum zuzuweisen (B), und tippen Sie auf Eingeben. Im selben Raum können bis zu 4 Relais konfiguriert werden.
  • Datos técnicos

    Sistema M y sistema D - Interruptor inalámbrico de una/dos teclas conectado – Guía del usuario del dispositivo Wiser Home

    Datos técnicos Datos técnicos Datos técnicos Batería CR2032 Vida útil de la batería Hasta 5 años (en función de la frecuencia de uso y la calidad de la batería) Clasificación IP IP20 Frecuencia de funcionamiento de 2405 a 2480 MHz Potencia de radiofrecuencia transmitida máx. <10 mW Alcance 100 m espacio abierto Temperatura de funcionamiento De -5 °C a 45 °C Humedad relativa Del 5 % al 95 % Protocolo de comunicación Zigbee 3.0
  • Resetting the device

    Wiser Radiator Thermostat – Wiser Home Device user guide

    for a few seconds until the center LED begins to flash red. Hold the cap in the “ -” direction until the LED flashes red 8 times. Release the cap; all 3 LEDs flash once indicating a successful reset of the Thermostat.
  • User interface lock settings

    Wiser Radiator Thermostat – Wiser Home Device user guide

    your room by playing with the Thermostat. To lock or unlock the Thermostat control: On the Home screen, tap . Tap Devices Radiator Thermostat Device lock toggle switch (A) to lock or unlock the Thermostat control. When the Thermostat lock is active, a (B) will appear next to Thermostat.
  • Repor o dispositivo

    Controlador/Barra de Conexão de Aquecimento de Piso Radiante Wiser – Guia do utilizador do dispositivo Wiser Home

    Repor o dispositivo Repor o dispositivo Repor o dispositivo Pode repor o Aquecimento do piso radiante para as predefinições de fábrica. Para repor o Aquecimento do piso radiante: Mantenha pressionado o botão Configuração durante mais de 15 segundos. Após 15 segundos, o LED pisca a vermelho. Quando o LED parar de piscar a vermelho, solte o botão de configuração. O LED para de piscar após uma reposição bem sucedida do Aquecimento do piso radiante.
  • Technical Data

    Wiser Boiler Relay – Wiser Home Device user guide

    Technical Data Technical Data Technical Data Mains voltage: AC 220-240 V, 50 Hz Switch rating: 2 (1) A, AC 230 V total load max. 2,5 A Wiring: Fixed wiring only User interface: 2x push button / LED Wired interfaces: 1x Relay output, 1x Digital boiler interface, 1x Wiser Boiler Relay power supply RF
  • Changing home Wi-Fi login information

    Wiser Home – System User Guide (Germany, Austria)

    change the Wi-Fi ® information in the hub: Tap I’ve changed my Wi-Fi router (A). The app will guide you through the process of selecting a Wi-Fi ® network and entering the password.
  • Energy Domain with Grid

    Wiser Home – System User Guide (Germany, Austria)

    Energy Domain with Grid Energy Domain with Grid Energy Domain with Grid If you have an energy device installed, like a PowerTag E, the Energy Centre will be available. In the Energy Centre, you can monitor your energy consumption and production, view detailed history, and get information on energy
  • Verlauf

    Wiser Home – Systemhandbuch (Deutschland, Österreich)

    können den angezeigten Zeitrahmen (Stunden, Tage, Monate und Jahre) durch Tippen auf (A) ändern. Grüne Balken zeigen die Solarstromerzeugung an, graue Balken zeigen den Batterieverbrauch an. Tippen Sie auf und wählen Sie Verbrauch aus, um den Energieverbrauch einzelner Lasten anzuzeigen. Tippen Sie erneut auf (A), um einen gewünschten Zeitrahmen auszuwählen.
Page 577 of 985