DUG_Radiator Thermostat_WH-07

User interface lock settings

Using the Wiser Home app, you can lock the Thermostat controls (nothing will happen when the Thermostat cap is twisted in either the + or – direction). This prevents children from changing the temperatures in your room by playing with the Thermostat.
To lock or unlock the Thermostat control:
  1. On the Home screen, tap .
  2. Tap Devices > Radiator Thermostat > Device lock toggle switch (A) to lock or unlock the Thermostat control.
    TIP: When the Thermostat lock is active, a (B) will appear next to Thermostat.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?