DUG_Radiator Thermostat_WH-07

Resetting the device

You can reset the Thermostat to factory default when it is attached to the radiator body. It can be reset manually at any time, e.g., when the Hub is replaced.

To reset the Thermostat:
  1. Twist and hold the cap in the “-” direction.
  2. Wait for a few seconds until the center LED begins to flash red.
  3. Hold the cap in the “-” direction until the LED flashes red 8 times.
  4. Release the cap; all 3 LEDs flash once indicating a successful reset of the Thermostat.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?