Showing 6,821 - 6,830 of 9,846 results

Page 683 of 985
  • Calibrage du volet avec l’application Wiser

    Odace - Interrupteur de commande de volet connecté – Guide de l'utilisateur de l’appareil Wiser Home

    la pièce où se trouve l'appareil. Sur l’écran de contrôle de l’appareil, faites glisser la barre coulissante vers le haut/vers le bas pour régler le pourcentage d’ouverture du volet souhaité (A). Le volet s’ouvre complètement, puis atteint la position souhaitée réglée à l’étape 2. Le volet est
  • Using the device

    EVlink Home Smart – Wiser Home device user guide

    Using the device Using the device Using the device The Control Panel allows you to start and stop charging and monitor the power consumption. On the Control page, tap EVlink Home Smart to access the control panel. On the control panel page, You can see the options A, B, C, D. Tap to see the options
  • LED indications

    Mureva EVlink – Wiser Home Device User Guide

    LED indications LED indications LED indications Pairing the device User Action LED Indication Status Press the push button 3 times LED blinks amber, once per second. Pairing mode is active for 30 seconds. When pairing is completed, LED displays solid green for a time, before turning Off. Resetting
  • Utilisation de l’appareil

    Mureva EVlink – Guide de l'utilisateur de l'appareil domestique Wiser

    page du panneau de contrôle, Vous pouvez voir les options A, B, C, D. Appuyez sur pour voir les options E, F, G, H, J. A Coût total de la session de facturation. B Durée totale de la charge dans la session. C Consommation totale d'énergie au cours de la session. D Bouton de commande (Démarrer la
  • Manage Wiser Home AI

    Wiser Home – System User Guide (Spain and Portugal)

    enrolled device to enable the new device. Dis-enroll the devices from Wiser Home AI: Disable the toggle switch for the devices you don’t want to have this feature. A notification window is prompted. Read the information carefully. If you wish to proceed, tap Continue, else tap Cancel. Changing your Home
  • Dispositivos de interligação sem Wiser Hub

    Sensor de fumo 230V Wiser – Guia do utilizador do dispositivo Wiser Home

    Dispositivos de interligação sem Wiser Hub Dispositivos de interligação sem Wiser Hub Dispositivos de interligação sem Wiser Hub Os sensores de fumo podem ser ligados diretamente entre si através de ligações de radiofrequência, mesmo sem uma rede Wiser Hub. Rode o interruptor de alimentação para a
  • Pairing 2-gang with 2 Blind Control Switches

    Exxact - Connected Blind Control Switch – Wiser Home Device user guide

    shutter will move up and down a few times during the pairing process. The status LED stops blinking green on the Wireless switch, and the blind control switch indicates that the pairing is successful. Check if the pairing was successful before you continue with the left channel. Short press the top-left
  • Laitteen pariliittäminen Wiser-keskusyksikön kanssa

    Exxact - Pistorasia 1-os. Zigbee – Wiser Home -laitteen käyttöopas

    , valitse Asenna ilman QR-koodia muodostaaksesi laiteparin manuaalisesti, ja jatka vaiheeseen 4. Jos QR-koodi on virheellinen, näkyviin tulee ilmoitus Virheellinen QR-koodi skannattu. Valitse En pysty skannaamaan QR-koodia, ja valitse jokin seuraavista vaihtoehdoista: (A): Kirjoita Mac-osoite/EUI-64 ja
  • Troubleshooting

    Airzone - Aidoo Pro Heat Pump – Wiser Home Device user guide

    connected to the same home network. The Aidoo is not updated with the latest firmware version. The Wi-Fi network is not powered ON. Solution: Use a Wi-Fi extender to make sure that your Aidoo receives a strong and stable connection. Power ON the Aidoo and connect to the same network as the Wiser Hub. Update
  • Automaation poistaminen

    Wiser 16A rele lämmityksen ohjaukseen – Laitteen käyttöopas

    Automaation poistaminen Automaation poistaminen Automaation poistaminen Lisätietoa Koti näyttö, napauta Automaatiot . Siirry kohteeseen Automaatio, napauta toimintoa, jonka haluat poistaa. Lisätietoa Muokkaa toimintoa näyttö, napauta Poista toiminto (A) ja lue vahvistusviesti ja napauta OK B).
Page 683 of 985