DUG_Exxact - Blind Control Switch_WH-01

Pairing 2-gang with 2 Blind Control Switches

To pair the 2-gang Wireless switch with 2 blind control switches, you must change your Wireless switch to 2-gang operation. Refer to Switching from 1-gang to 2-gang operation.
NOTE: Do not remove the rocker of the blind control switches.
  1. Short press the right upper push button 5 times in quick succession on the Wireless switch.
    The status LED blinks green.

  2. Short press the first blind control switch 5 times in quick succession.
    The status LED blinks green.

    The shutter will move up and down a few times during the pairing process. The status LED stops blinking green on the Wireless switch, and the blind control switch indicates that the pairing is successful.
    IMPORTANT: Check if the pairing was successful before you continue with the left channel.
  3. Short press the top-left push button 5 times in quick succession on the Wireless switch.
    The status LED blinks green.

  4. Repeat step 2 on the second blind control switch.
    The shutter will move up and down a few times during the pairing process. The status LED stops blinking green on the Wireless switch, and the blind control switch indicates that the pairing is successful.
  5. Set up the shutter calibration manually. For more information, refer to shutter calibration without wiser app.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.