DUG_Unica Shutter_WH-08

Pairing 2-gang with 2 Blind Control Switches

To pair the 2-gang Wireless switch with 2 blind control switches, you must change your Wireless switch to 2-gang operation. Refer to Switching from 1-gang to 2-gang operation.
  1. Remove the rocker from the Wireless switch.
  2. Short press the top-right push button 5 times in quick succession on the Wireless switch.
    The status LED blinks green.
  3. Short press the first blind control switch 5 times in quick succession.
    The status LED blinks green.
    The shutter will move up and down a few times during the pairing process. The status LED stops blinking green on the Wireless switch, and the blind control switch indicates that the pairing is successful.
    IMPORTANT: Check if the pairing was successful before you continue with the same channel.
  4. Short press the top-left push button 5 times in quick succession on the Wireless switch.
    The status LED blinks green.
  5. Repeat step 3 on the second blind control switch.
    The shutter will move up and down a few times during the pairing process. The status LED stops blinking green on the Wireless switch, and the blind control switch indicates that the pairing is successful.
  6. Set up the shutter calibration manually. For more information, refer to shutter calibration without wiser app.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?