DUG_Unica Shutter_WH-08

Operating the device manually

  • Long press the blind control switch (> 0,5 s) to move the shutter up or down (A).

    • Press (ʌ) to open the shutter.

    • Press (v) to close the shutter.

  • Short press (<0,5 s) to stop the moving shutter (B).
  • For shutter with tilting slats: When the shutter is not moving short press (<0,5 s) the blind control switch to adjust the slat position (C).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?