DUG_Unica Shutter_WH-08

Removing the device from Wiser system

Using the Wiser app, you can remove the blind control switch from the system.
To remove the device:
  1. On the Home screen, tap .
  2. Tap Devices > Shutters > Blind control switch or Shutter slat > Delete (A).
    NOTE:
    • Removing the device will reset the blind control switch. The LED starts blinking amber indicating that the blind control switch is ready for pairing.

    • If there is a problem while pairing or resetting the blind control switch, refer to Resetting the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?