DUG_Unica Shutter_WH-08

Troubleshooting in Quick Home Connect

Symptom

Possible cause

Solution

LED displays amber on the device.

Pairing not completed and returned to factory default.

Pair the Wireless switch and the device again.

Refer to

Wireless switch not able to control the device reliably.

The Wireless switch and the device are too far away from each other.

Place the Wireless switch in a position closer to the device.

The Wireless switch lost pairing.

Pair the device again.

Refer to

The Wireless switch battery is discharged.

Replace the battery of the Wireless switch

Scenario

Procedure

Control multiple devices with one Wireless switch.

To control multiple devices with a single Wireless switch, start by pairing it with one device. Then, use the same Wireless switch to pair with additional devices.

NOTE: You can pair up to 7 devices to a single Wireless switch.

1-gang FLS with devices (relay switch, dimmer, shutter control, or socket outlet).

Pair the Wireless switch with any of the devices (relay switch, dimmer, shutter control, or socket outlet).

2-gang FLS with devices (relay switch, dimmer, shutter control, or socket outlet).

Pair either left or right Wireless switch with any of the devices (relay switch, dimmer, shutter control, or socket outlet). You can also pair another rocker of the Wireless switch with another device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?