DUG_Multiwire Puck Dimmer_WH–01

Removing the device from Wiser system

Using the Wiser app, you can remove the dimmer from the system.
  1. On the Home page, tap .
  2. Tap Devices > Micromodule Dimmer > Delete (A).

    NOTE:
    • Removing the device will reset the dimmer. After reset the LED turns amber indicating that the dimmer is ready to pair with another network.

    • If there is a problem while pairing or resetting the dimmer, refer to Resetting the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?