DUG_Multiwire Puck Dimmer_WH–04

Connected Light Control

You can set up commands for turning on/off and dimming up/down the lights using the push-button switch.
  1. Select Connected Light Control from the slide up menu.
  2. Tap the option that you want to configure.
    • Turn On/Off, Dim Up/Down: The light can be turned on/off by short pressing the push button, and the brightness of the light can be increased/decreased by pressing and holding the push button.
    • Turn On, Dim Up: The light can be turned on by short pressing the push button, and the brightness of the light can be increased by pressing and holding the push button.
    • Turn Off, Dim Down: The light can be turned off by short pressing the push button, and the brightness of the light can be decreased by pressing and holding the push button.
  3. Once the option is selected, tap Save.
    IMPORTANT:
    • If you have configured a push button with the Turn On, Dim Up option, you can use it to both turn on the light and increase its brightness. However, to turn off the light and reduce its brightness, you should configure another push button with the Turn Off, Dim Down option, or you can perform these actions using the app.

    • If you have configured a push button with the Turn Off, Dim Down option, you can use it to both turn off the light and decrease its brightness. However, to turn on the light and increase its brightness, you should configure another push button with the Turn On, Dim Up option, or you can perform these actions using the app.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.