Pairing Wireless Switch with Multiwire Micro Module Dimmer
- Short press the upper push button 5 times in quick succession on the Wireless switch.
-
Follow either of the options to pair the Dimmer:
WARNINGHAZARD OF ELECTRIC SHOCK- Observe the regulations for working on live parts.
- Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.- Short press the Setup/Reset button 5 times in quick succession on the Dimmer.
- Short press the left push button (Wired to terminal 1) 5 times in quick succession.
The status LED blinks green on the Dimmer.NOTE: If the Dimmer is located behind the mechanical push-button, the status LED is not visible.The light connected to the Dimmer blinks for a few times. The status LED stops blinking green on the Wireless switch and the Dimmer. The Dimmer can now be controlled by the Wireless switch.