DUG_Multiwire Puck Dimmer_WH–04

Setting up the Power On Behaviour

You can configure the dimmer brightness level when turned on.
  1. On the Home screen, tap .
  2. Tap Devices > Micromodule Dimmer > Power On Behaviour (A).
  3. Select one of the following options as per your preference:

    Last On Brightness Level: The light turns on at the same brightness as when it was last turned off (also called Memory).

    Specific Brightness Level: This option allows you to get the desired brightness level every time you turn on the light. Drag the slider bar to set the brightness.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?