Configuring the device
|
A |
Device Name: Tap to change the name of the device. |
|
B |
Location: Tap to assign the Dimmer to any room (such as living room, bedroom, kitchen etc). Refer to Setting the device location for more details on how to set the location. |
|
C |
Dimming mode: You can improve the dimming quality in the app if you have problems with light flickering. Refer to Setting Dimming Mode for detailed information on setting the dimming mode. |
|
D |
Power On Behaviour: Tap to set the default brightness level of the dimmer when it is turned on. Refer to Setting up the Power On Behaviour for detailed information on each options. |
|
E |
Configure Connected Switches: This setting allows you to configure the push-button switches of the dimmer to different functions. Refer to Configure Connected Switches for detailed information on each function. |
|
F |
BRIGHTNESS LEVELS: This setting lets you set limits on the maximum and minimum brightness
of the light. This is done to avoid flickering and switching off the
LED. IMPORTANT: If the light does not begin to brighten up from 0%,
adjust the minimum level setpoint to the point where the light actually
starts to brighten. Similarly, for maximum brightness, set the maximum
level based on the behaviour of the connected light. For example,
if brightness does not increase between 80% and 100%, then set the
maximum level to 80%.
NOTE: The minimum brightness must be
lower than the maximum brightness.
|
|
G |
Neutral wire fitted: The Wiser app automatically detects the wiring mode based on the installation, eliminating the need for manual selection. Yes, if installed with a neutral wire, NO if installed without a neutral wire. |
|
H |
Identify: Tap
to identify the device. The status LED blinks red and connected lighting
devices blinks On/Off, upon successful identification of the dimmer. |
|
J |
Delete: Tap to remove the device from the system. NOTE:
|
|
K |
Zigbee Signal Strength Indicator: Zigbee Signal Strength indicator displays the current signal strength of the device. |