DUG_Multiwire Puck Dimmer_WH–01

Setting Brightness level

Using the Wiser Home app, you can set the minimum and maximum brightness level.
  1. On the Home page, tap .
  2. Tap Devices > Micromodule Dimmer.
  3. Drag the slider bar to increase or decrease the Minimum Brightness and Maximum Brightness (A).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?