DUG_Wiser_Micromodule for Fil Pilote radiators_WH-05

Using the device

The Device Control Screen allows you to switch ON/OFF the device and control various settings.

On the Control tab, select the tap All devices or a room tab where the module is located > Heating device

The Device Control Screen displays the following options:


A

Drag the sliding bar up/down to adjust the set-point temperature (Heating).

B

Tap to change the operating mode. for more information, refer to Operating modes

C

Tap to redirect you to the Schedule screen, where you can create a schedule. For more information, refer to the Creating a schedule topic.

D

Add to favourites Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide..

E

Tap to control various settings from the Room Settings screen. For more information, refer to the Configuring the device topic.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?