DUG_Wiser_Micromodule for Fil Pilote radiators_WH-05

Resetting the device

You can reset the device to factory default manually.
Short press the Setup/Reset button of the module 3 times and then long press once (>10 s) on the module.

    QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

    Was this helpful?