SUG_NL_WH-04

Limitations of the Wiser System

When commissioning a Wiser system, it is important to understand the system limits, such as the maximum number of supported devices.

System Limits

Maximum number of  

Devices Zigbee

63

Hub

1

PowerTag E

20

Rooms

16

Moments

20

Automations

10

Energy

Maximum overall

Maximum per Room

PowerTag E

20

-

PowerTag C

20

-

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.