SUG_NL_WH-04

Downloading hub firmware into the app

When the hub is connected to the Wiser cloud, it automatically updates the latest firmware.

If you want to update the hub manually before connecting to the cloud, you can use the app as a professional installer.

IMPORTANT: The Hub firmware download is available only for the Wiser Hub 2nd Generation.

As a professional installer:

  1. Tap Hub Firmware (A).

  2. Tap Check for updates (B).

  3. If there is a new version of firmware, it will be downloaded into the app.

NOTE: If a firmware is saved in the app, you can check the version number and expiry date.
  • To check if a newer version is available, tap Update firmware (A).

  • To remove a firmware from your app, tap the bin (B).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.