SUG_NL_WH-04

App Settings

Overview of the options available in the settings menu.

The settings menu contains various settings for parts of the Wiser Home System.

Rooms and Devices are managed from the settings menu.

On the Home Screen:

  1. Tap .

    The settings menu:

    Account

    Change the details of your account, like password, notification settings, home address, etc.

    NOTE: You can also find the notification settings (e.g. Battery low) here.

    Energy Management

    This option is available only if you have Energy devices installed at your home.

    • Tariff: Set the tariff to access your energy cost and billing data. You can set the tariff based on your contract type. Refer to Setting Tariff for detailed information on how to set the tariff.

    Rooms

    List of all Rooms of your Home. Access to Room options.

    Devices

    List of all Devices of your Home. Access to Device options.

    Away Mode

    Specify what happens when you activate the Away Mode, like temperature setting and which devices should be switched off. Refer to Away Mode for detailed information.

    System Settings

    More detailed Wiser Home App information. Set your time zone here.

    Support

    Provides you the general assistance such as the link to the FAQ section of , access detailed guide, report errors, and provides contact information for customer support. Refer to Support for the detailed information.

    Home Screen

    Customize the appearance of the Home Screen.

    App Theme

    Personalize the appearance of Wiser home app to light mode or dark mode. Refer to App Theme.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.